Overslaan naar hoofdinhoud

Classic Switch v09.0.18 released (MACH1040 and MACH 104) - Nieuws / Switches and Router - Belden Support Center

mei 20 2019

Classic Switch v09.0.18 released (MACH1040 and MACH 104)

Lijst van auteurs

Classic Switch software 09.0.18 has been released for MACH 1040 and 104.
This version fixes a link issue in cobination with SFPs:

In certain scenarios when unplugging a fiber link from a port also the neighbor port is going down