Overslaan naar hoofdinhoud

HiLCOS 10.34 Release Update 4 - Nieuws / Wireless - Belden Support Center

mei 5 2023

HiLCOS 10.34 Release Update 4

Lijst van auteurs

Hirschmann is proud to announce the release of HiLCOS 10.34 Release Update 4:

https://hirschmann-support.belden.com/downloads/files/3839

For the devices:

  • OpenBAT (BAT-F and BAT-R)
  • BAT450-F (all variants, except LTE)
  • BAT867-R and BAT867-F
  • BAT Controller Virtual and BAT WLC


Download also contains complementary software LANConfig and LANMonitor

Feature and bugfix highlights

Full list of new features can be found in the release notes in the zip file.

  • Improved BAT867 radio stability
  • Added trace messages for access point mode in case of connectivity issues between the
    access point & client
  • GPS output now is shown with increased accuracy (additional decimal)
  • Fixed Configuration Upload and Download function compatibility for Industrial HiVision Tool
  • PMK Lifetime parameter is now configurable on WLAN Controller
  • Firewall for IPv4 enabled by default
  • Default value of TCP max connection has been updated to 200 for all BAT devices except WLC