Overslaan naar hoofdinhoud

HiView v03.1.01 released - Nieuws / Software Products - Belden Support Center

feb 8 2019

HiView v03.1.01 released

Lijst van auteurs

New features in version 03.1.01

  • HiView now offers two options for application installation. You can still download the zip file, and a new installation wizard has been added.

Fixed in 03.1.01

  • The graphical user interface of the BRS device can now be open using the latest version of the HiView application.